Below are definitions for the product environmental compliance terms used on TE.com:
- EU RoHS Directive 2011/65/EU
- EU ELV Directive 2000/53/EC
- China RoHS 2 Directive MIIT Order No 32, 2016
- EU REACH Regulation (EC) No. 1907/2006
- Halogen Content
EU RoHS Directive 2011/65/EU
Compliant
These products comply with the substance restrictions of the Restriction on Hazardous Substances Directive 2011/65/EU (RoHS2). The RoHS2 Directive requires that certain electrical and electronic equipment products do not contain mercury, cadmium, hexavalent chromium, PBB, PBDE, lead, DEHP, BBP, DBP and DIBP above defined thresholds. Products indicated as 'Compliant' do not contain any of these substances above the prohibition thresholds. Finished electrical and electronic equipment products will be CE marked as required by the Directive. Components may not be CE marked.
Compliant with Exemptions
These products comply with the substance restrictions of the Restriction on Hazardous Substances Directive 2011/65/EU (RoHS2). The RoHS2 Directive requires that certain electrical and electronic equipment products do not contain mercury, cadmium, hexavalent chromium, PBB, PBDE, lead, DEHP, BBP, DBP and DIBP above defined thresholds. Products indicated as 'Compliant with Exemptions' contain one or more of these substances above the prohibition thresholds, but are compliant by claiming one or more valid exemptions. Finished electrical and electronic equipment products will be CE marked as required by the Directive. Components may not be CE marked.
Not Compliant
These products DO NOT comply with the substance restrictions of the Restriction on Hazardous Substances Directive 2011/65/EC (RoHS2). Products indicated as 'Not Compliant' contain one or more restricted substances above the prohibition thresholds. Consequently, these products should NOT be used in any application requiring RoHS2 compliance.
Out of Scope
These are products that TE Connectivity considers to be out of scope for the Restriction on Hazardous Substances Directive 2011/65/EU (RoHS2). Products indicated as 'Out of Scope' typically are not electrical or electronic in nature, nor would be used in electrical/electronic equipment covered by this Directive. Customers should verify this assessment prior to use.
Not Yet Reviewed
These products have not yet been reviewed for compliance with the Restriction on Hazardous Substances Directive 2011/65/EU (RoHS2).
The 4 Phthalates DEHP, BBP, DPB and DIBP added by amendment 2015/863/EU became restricted as of 22 July 2019 for all electrical and electronic equipment, apart from Categories 8 (medical devise) and 9 (monitoring and control equipment) for which the restriction applies as of 22 July 2021.
EU ELV Directive 2000/53/EC
Compliant
These products comply with the substance restrictions of the End of Live Vehicles Directive 2000/53/EC (ELV). The ELV Directive requires that materials and components of vehicles do not contain mercury, cadmium, hexavalent chromium, and lead above defined thresholds. Products indicated as 'Compliant' do not contain any of these substances above the prohibition thresholds.
Compliant with Exemptions
These products comply with the substance restrictions of the End of Life Vehicles Directive 2000/53/EC (ELV). The ELV Directive requires that materials and components of vehicles do not contain mercury, cadmium, hexavalent chromium, and lead above defined thresholds. Products indicated as ' Compliant with Exemptions' contain one or more of these substances above the prohibition thresholds, but are compliant by claiming one or more valid exemptions.
Not Compliant
These products DO NOT comply with the substance restrictions of the End of Life Vehicles Directive 2000/53/EC (ELV). Products indicated as 'Not Compliant' contain one or more restricted substances above the prohibition thresholds. Consequently, these products should NOT be used in any application requiring ELV compliance.
Out of Scope
These are products that TE Connectivity considers to be out of scope for the End of Life Vehicles Directive 2000/53/EC (ELV). Products indicated as 'Out of Scope' typically are not materials or components of vehicles. Customers should verify this assessment prior to use.
Not Yet Reviewed
These products have not yet been reviewed for compliance with the End of Life Vehicles Directive 2000/53/EC (ELV).
China RoHS 2 Directive MIIT Order No 32, 2016
China RoHS - Environmental Friendly Use Period (EFUP) Symbol
EFUP E (see green label below): No hazardous material exists over the threshold of GB/T 26572-2011 standard - China's Requirements for Concentration Limits for Certain Hazardous Substances in Electrical and Electronic Products.
EFUP 10 (see orange label below): Hazardous material exists over the threshold of GB/T 26572-2011. The number shown in the center of the symbol indicates the Environmental Friendly Use Period as defined by SJ/T 11364-2014 – China's Marking for the Restriction of the Use of Hazardous Substances in Electrical and Electronic Products.
Note: EFUP 10 is an example only. EFUP values (shown in the center of the symbol) may vary by product family/part.


EU REACH Regulation (EC) No. 1907/2006
Current Candidate List
Indicates the Month / Year of the current, authentic version of the Candidate List of Substances of Very High Concern (SVHC) as published by the European Chemicals Agency (ECHA).
Candidate List Declared Against
Refers to the Month / Year of the version of the Candidate List of Substances of Very High Concern (SVHC) published by the European Chemicals Agency (ECHA) at the time the product was last reviewed by TE for SVHC.
Does Not Contain REACH SVHC
These products do not contain Substances of Very High Concern (SVHC) > 0.1% by weight (1000 ppm).
SVHC > Threshold
These products contain one or more EU REACH Substances of Very High Concern (SVHC) > 0.1% by weight (1000 ppm). Details related to the SVHC are displayed.
Not Yet Reviewed
These products have not yet been reviewed to determine whether they contain any Substances of Very High Concern (SVHC).
Halogen Content
Low Halogen
These products contain less than 900 ppm of each Bromine, Chlorine and Fluorine, and less than 1500 ppm of Bromine + Chlorine per homogenous material. Products meet Low Halogen definitions in all following industrial standards: IEC 61249-2, IPC-4101, JPCA-ES-01, JEDEC/ECA joint Standard JS709A and military standard MIL-C-24643 on low smoke zero halogen (LSZH). Products also meet the definitions of Low Bromine/Chlorine and BFR/CFR/PVC Free.
Low Bromine/Chlorine
These products contain less than 900 ppm of Bromine and Chlorine, and less than 1500 ppm of Bromine + Chlorine per homogenous material. May contain Fluorine or content of Fluorine is unknown. Product meet Low Halogen definitions in all following industrial standards: IEC 61249-2, IPC-4101, JPCA-ES-01 and JEDEC/ECA joint Standard JS709A. Product do NOT meet Low Halogen definitions in military standard MIL-C-24643 on low smoke zero halogen (LSZH). Products also meet definition of BFR/CFR/PVC Free.
BFR/CFR/PVC Free, but Br/Cl >900 ppm in other sources
These products do not contain Brominated Flame Retardant, Chlorinated Flame Retardant or PVC, but contain more than 900 ppm of Bromine and Chlorine in sources other than BFR/CFR/PVC; may also contain Fluorine. Product meet Low Halogen definition in JEDEC/ECA joint Standard JS709A. Product do NOT meet Low Halogen definitions in IEC 61249-2, IPC-4101, JPCA-ES-01 and military standard MIL-C-24643 on low smoke zero halogen (LSZH).
Not Low Halogen
These products contain Brominated Flame Retardant or Chlorinated Flame Retardant or PVC and may also contain Fluorine. Product do NOT meet Low Halogen definitions in all following industrial standards: IEC 61249-2, IPC-4101, JPCA-ES-01, JEDEC/ECA joint Standard JS709A and military standard MIL-C-24643 on low smoke zero halogen (LSZH).
Out of Scope
These products are specifically excluded from Low Halogen requirements.
Not Reviewed for Halogen Content
These products have not yet been reviewed to determine Halogen content.