TE Connectivity launches new Linx CW-RCS series Wi-Fi 6/6E/7 right-angle whip antennas.
Published
05/04/23
Media Inquiries
David Lang
TE Connectivity
+1 (717) 216-9150
david.lang@te.com
MERLIN, Oregon
May 4, 2023
New CW-RCS series Wi-Fi 6/6E/7 compact, right-angle whip antennas from Linx Technologies (Linx), now a part of TE Connectivity (TE), a world leader in connectors and sensors, provide customers with the capability to use the popular CW-RCS profile antenna for Wi-Fi 6/Wi-Fi 6E/Wi-Fi 7 applications in the 2.4 GHz, 5 GHz and 6 GHz bands.
“This new product offering adds a compact, reduced-height whip style antenna to our expanding portfolio of Wi-Fi antenna products," said Ganesh Srinivasan, TE vice president of business development and marketing. "This enables customers to use this popular low-profile antenna form factor in Wi-Fi applications.”
The ANT-W63-CW-RCS is a compact, reduced-height monopole whip antenna with a length of only 54 mm that may be used with metallic and non-metallic enclosures. The right-angle rotating design of the ANT-W63-CW-RCS antenna allows for the antenna to be positioned for optimum performance.
The antennas connect via an SMA plug (male pin) or RP-SMA plug (female socket) connector.
The new offering is available now via Linx Technologies’ distributor and manufacturer representative networks. For larger quotes, contact TE Connectivity at: contact.linx@te.com.
For more information about these antennas, visit: https://linxtechnologies.com/wp/product/w63-cw-rcs-wifi-antenna/
ABOUT LINX TECHNOLOGIES
Linx Technologies (now part of TE Connectivity) strives to Make Every Engineer a Hero in Record Time by minimizing the risk, delays, and technical challenges for design engineers to make products wireless and connect them to the Internet of Things (IoT). Linx manufactures wireless components including antennas, RF connectors and cables, RF modules, and remote controls. Linx relentlessly focuses on customer success. Every aspect of the Linx Technologies business offers Wireless Made Simple products, including the documentation, support, and design experience.