TE News: TE Connectivity’s STD Snap-On Markers

TE Connectivity’s STD Snap-On Markers designed for identifying wires in harsh environments

Published

01/24/19

Media Inquiries

Jonathan Graham

Email - jonathan.graham@te.com

Tel -  +49-6151 607 3756

DARMSTADT, Germany

Jan. 24, 2019

TE Connectivity (TE), a world leader in connectivity and sensors, is offering its STD Snap-On Markers as a reliable way to identify wires and small cables.

Manufactured with a zero halogen polyoxymethylene compound, these expanding profile markers are side-entry installed using an applicator wand, allowing identification after termination and/or installation.

 

“With its excellent resistance to burning and no halogen, TE snap-on markers are the perfect way to permanently and rapidly mark cables and wires, both before and after termination and installation in harsh environments,” said Thomas Bartlett, TE product manager. “Also, the STD markers are made from polyoxymethylene which guarantees strength, dimensional stability, low moisture absorption, and good resistance to chemicals.”

 

Markers are side-entry installed using an applicator wand, allowing identification after termination and/ or installation. These markers have an expanding profile which enable markers to accommodate a wide range of wire and small cable sizes. Markers are supplied with a “chevron” cut to ensure the legend remains aligned. TE’s STD snap-on wire markers are designed to stand the test of time, preventing costly re-work before the life of the equipment ends.

 

“With its UL94 rating and durability in operating temperatures from  -40°C  to 106°C (-40ׄ°F – 223°F), the STD marker is ideal for field operations including power stations, oil refineries and offshore platforms,” said Bartlett.