Interactive Display at electronica Trade Fair
Published
11/07/16
Media Inquiries
Keith Myers
TE Connectivity
919-557-8893 tel
Keith.Myers@te.com
The Simon Group
Beth Smith
215-453-8700 tel
Bsmith@simongroup.com
BERWYN, Pa – November 7, 2016 – TE Connectivity (TE), a world leader in connectivity and sensors, will showcase its wireless pressure sensing technology with an interactive display spanning two booths at the electronica trade fair in Munich, Germany, from November 8-11.
Wireless sensors at the TE Connectivity Sensors (TESS) exhibit (B1.233) will remotely monitor barometric pressure, humidity, temperature and proximity at TE’s main exhibit (B2.225) via smart badges, with data displayed at the TESS exhibit. Using a simple computer interface, wireless sensors across several different industrial markets will remotely track environmental changes to improve productivity and identify any problems before a failure occurs.
Also on display will be a number of key sensor technologies for industrial applications, including test and measurement, and microelectromechanical-based (MEMS) waterproof altimeters for liquid or gas pressure measurement. TE will also feature ‘header-less’ media-isolated digital output sensors that offer low cost and high temperature performance. All sensors can be used in a wide range of applications in the harshest conditions.
Sensors in the Connected Factory Presented at IT2Industry@electronica
On Tuesday, November 8, during the IT2 Conference held in conjunction with electronica, Dave Enright, Field Application Engineer, TE Connectivity, will discuss the role sensors play in Industrial IoT and the Connected Factory. For more information, please attend the presentation at 2:40 p.m. (Hall Eingang West) or visit our exhibit during the show.
Enright notes, “We’re excited to present at the show and help drive innovation across industries and applications – from automotive and industrial IoT to the connected lifestyle. TE’s breadth and depth of sensor technology and engineering prowess have helped reinforce our commitment to all these growth markets to improve safety, performance and environmental standards as well as business and process efficiencies.”
With engineering expertise in areas as diverse as the connected home, the connected car and theconnected factory, TE is helping to enable a connected life by sensing data, power and signals in areas never before possible. Offering one of the broadest sensor portfolios in the industry, the company meets a wide range of application needs through customized solutions and close customer collaboration.
TE’s sensor technologies are capable of measuring vibration, shock, pressure, force, humidity and position throughout product research, test and evaluation and developmental purposes for high reliability and performance in harsh environmental conditions.
TE Connectivity provides its customers with a broad set of sensor and connector solutions, advanced manufacturing and excellent engineering talent through a continued focus on innovation and harsh environments.