Medical Technologies
On April 29, 2024, the U.S. Food and Drug Administration (FDA) published a final rule on the enforcement and oversight of laboratory-developed tests (LDTs), effective July 5, 2024. The final rule amends its regulations to make explicit that IVDs are devices under the Federal Food, Drug, and Cosmetic Act (FD&C Act), including when the manufacturer of the IVD is a laboratory. An LDT is an in vitro diagnostic (IVD) product developed, manufactured, and used inside a single laboratory certified under the Clinical Laboratory Improvement Amendments of 1988 (CLIA) and meets the CLIA requirements to perform high-complexity testing. The publication of this rule marks the end of a long-standing policy by the FDA to exercise enforcement discretion over LDTs, meaning it has[GM3] [DT4] largely not exercised its ability to regulate these tests. The final rule establishes a timeline for LDT manufacturers to comply with FDA IVD requirements. This justification is based on many laboratory-manufactured tests, for example, being developed with the same materials, technologies and scientific concepts as well as requiring the same level of experience and/or training to operate, as IVDs from conventional manufacturers. Also, many LDT developers and IVD companies manufacture tests intended for the same or similar purpose, thus targeting patients with similar health concerns. Consequently, with few exceptions, LDT developers will overtime be held to the same requirements and FDA regulations as traditional IVD companies.
A large portion of the final rule lays out why the FDA has the legal authority to regulate LDTs, and the history around why it has changed its stance on exercising enforcement discretion over LDTs. It is noted that a lot has changed since the Medical Device Amendments (MDA) were originally enacted in 1976, and with how LDTs have evolved, there are considerable questions about the safety and effectiveness of many LDTs currently available in the market. Moreover, it is important to recall that the FDA has spent the past four years requiring LDTs for SARS-CoV-2 and more recently with Mpox, to obtain emergency use authorization (EUA) after an initial review of analytical and clinical validation data. Perhaps this requirement was a prelude to the coming LDT regulatory enforcement, and an opportunity for both labs and the FDA to prepare for this expanded oversight role on LDTs.
It is important to point out that not all LDTs will be subject to FDA oversight and review. The FDA does carve out a few exceptions to the end of the enforcement discretion on LDTs. These exceptions include:
Other exceptions to the end of the FDA’s enforcement discretion are listed below. For the below exceptions, laboratories must still follow design controls and other quality system (QS) [MR1] [TD2] requirements for the modification, as the exception is only to the requirement for a premarket review.
then the FDA will expect the laboratory developer to comply with the premarket review and QS requirements for the modified LDT.
The final rule outlines a gradual phase-out of the enforcement discretion for applicable LDTs over a period of four years. There are five stages to the rollout.
The end of the enforcement discretion on LDTs by the FDA may catch laboratory
manufacturers by surprise. It has been anticipated for some time, but labs may
not have familiarity with the FDA’s regulatory pathways, data requirements, and
submissions. As a result, TE Connectivity’s (TE) IVD Solutions team would like
to offer a few recommendations on what LDT developers could consider when
deciding their next steps:
The IVD Solutions team at TE is experienced in helping IVD manufacturers achieve
FDA clearance/approval for IVDs with a variety of intended uses. Should you
need assistance navigating the latest FDA oversight, the IVD Solutions team at TE can assist.
For Informational Purposes Only. Individual circumstances vary. This information is provided for promotional or general informational purposes only and is not to be relied upon as a professional opinion or advice. No reader should act or refrain from acting on the basis of this information without first seeking advice from a qualified professional.