Condition Monitoring Sensors

Application

INDUSTRIAL CONDITION MONITORING

Learn how predictive maintenance sensors help anticipate machine failures, increase productivity, lower maintenance costs, and improve worker safety.

While condition monitoring has been around for years, it is evolving with the Internet of Things (IoT).  This growth of IoT, and its advancing ecosystem which supports continuous monitoring in all factory assets, has affected condition monitoring practices and has contributed to evolving predictive maintenance operations. Sensors are now being manufactured to include the requirements demanded by this IoT ecosystem. The latest sensor developments are being influenced by IoT trends such as miniaturization, digitization, sensor fusion, low power and wireless technologies while being packaged for harsh environments. As a result, sensors are progressing to enable continuous condition monitoring by collecting data which facilitates intelligent decisions via machine learning or artificial intelligence (AI). Vibration, pressure, position, speed, fluid property, temperature and humidity sensors all play a critical role within industrial condition monitoring applications. These industrial sensors help reduce downtime by predicting machine failures, increasing productivity, lowering maintenance costs, and improving worker safety.

Value of condition monitoring infographic

Industrial condition monitoring sensors historically have been used for heavy, high-end machinery such as windmills, industrial pumps, compressors, and HVAC systems. However, with the shift in IoT and increased automation practices, there is a need for adding condition monitoring sensors onto smaller systems such as machine spindles, conveyor belts, sorting tables, and machine tools which require better predictive maintenance. Reducing machine downtime in these industrial applications is a critical consideration in terms of customer experience and profitability. Therefore, the value of implementing condition monitoring and preventive maintenance practices include many benefits which would not be realized without the use of accurate, reliable sensors. With the proper sensor to measure the needed data, condition monitoring could be accomplished within any industrial application and predictive maintenance can take place to confirm that operations can stay up and running when needed.

  1. Revolutionizing Industry 4.0: Advanced Vibration Sensing by TE Connectivity

Explore the future of Industry 4.0 with TE Connectivity's advanced vibration sensors. Join Bernard Kamel, TE Connectivity's Wireless Sensor Engineering Manager, for an insightful journey into how these innovative devices are reshaping maintenance and monitoring practices. Understand their pivotal role in preventing equipment failure and enhancing system performance. Delve into a realm where predictive maintenance aligns with state-of-the-art technology.

Sensors for Predictive Maintenance in Harsh Environments
On-Demand Webinar

Learn how sensors can be used in predictive maintenance and the added value of recognizing sensors as key components of condition monitoring applications. These industrial sensors help predict machine failures, increase productivity, lower maintenance costs, and improve worker safety in harsh environments.

Sensors for Predictive Maintenance in Harsh Environments
On-Demand Webinar

Learn how sensors can be used in predictive maintenance and the added value of recognizing sensors as key components of condition monitoring applications. These industrial sensors help predict machine failures, increase productivity, lower maintenance costs, and improve worker safety in harsh environments.

Condition Monitoring Sensors
Enabling Industry 4.0 Webinar

While condition monitoring has been around for years, it is evolving with the Internet of Things (IoT). Watch this webinar to discover how IoT is evolving, how condition monitoring sensors are enabling this shift, and the value of recognizing sensors as key components of condition monitoring applications. 

Condition Monitoring Sensors
Enabling Industry 4.0 Webinar

While condition monitoring has been around for years, it is evolving with the Internet of Things (IoT). Watch this webinar to discover how IoT is evolving, how condition monitoring sensors are enabling this shift, and the value of recognizing sensors as key components of condition monitoring applications. 

Reducing Costly Downtime: Accelerometers Transform Machine Maintenace
On-Demand Webinar

Factories are becoming more autonomous and require sensors to monitor equipment on the factory.  Watch this webinar to learn how sensors are capturing critical data for performance analytics, improved efficiency, lower costs, and better equipment utilization.

Reducing Costly Downtime: Accelerometers Transform Machine Maintenace
On-Demand Webinar

Factories are becoming more autonomous and require sensors to monitor equipment on the factory.  Watch this webinar to learn how sensors are capturing critical data for performance analytics, improved efficiency, lower costs, and better equipment utilization.

  1. The Power of IoT Wireless Pressure Sensors

TE Connectivity's 65xxN & 69xxN series wireless pressure sensors bring practical innovation to industrial monitoring. Engineered with LoRaWAN® and Bluetooth® technology, these compact sensors fit seamlessly into various environments, from tight spaces to remote infrastructures. They offer a wide pressure sensing range, reducing the need for multiple sensors and simplifying system integration, with an impressive battery capacity of 2100 mAh. Watch this product introduction video now, for a more efficient approach to modern industrial monitoring.

FREQUENTLY ASKED QUESTIONS

1

What is industrial condition monitoring?

Condition monitoring is the method of assessing components within industrial equipment to identify any changes that occur within the machinery which typically indicates there is a problem. If there is a significant change detected, this could signal the need for maintenance.

2

What is predictive maintenance?

Predictive maintenance is a subset of condition monitoring that focuses on determining when maintenance needs to be performed on industrial equipment and machinery. It enables uptime for manufacturing factories and allows for continuous development of goods to confirm positive customer experiences and profitability.

3

Do sensors enable condition monitoring and predictive maintenance?

Yes, by placing sensors on industrial equipment to monitor performance, identify changes in different parameters, and determine if changes signal a need for equipment maintenance enables the practice of condition monitoring and/or predictive maintenance. Sensors are progressing to facilitate continuous condition monitoring by collecting data which helps in making intelligent decisions via machine learning or artificial intelligence (AI).