TE Connectivity’s Analog Infrared Thermopile temperature sensors provide a non-contact, high-precision temperature measurement solution
Published
02/08/21
TAIPEI, China – Feb. 8, 2021
TE Connectivity’s Analog Infrared Thermopile temperature sensors provide a non-contact, high-precision temperature measurement solution
Sensors are designed to measure temperature from a distance by detecting an object's emitted infrared energy
TAIPEI, China – Feb. 8, 2021 – As medical and industrial markets evolve, there is a high demand for accurate, non-contact temperature measurement. TE Connectivity (TE), a world leader in connectivity and sensors, manufactures non-contact Analog Infrared Thermopiles to support a wide range of accuracy, packaging and performance requirements to meet the needs of these evolving industries and to help create a safer, sustainable, productive and connected future.
Thermopile sensors are designed to measure temperature by detecting an object's emitted infrared energy from distances a fraction of an inch to several feet away. The thermopile sensing element, composed of small thermocouples on a silicon chip, absorbs the energy and produces an output signal.
“Providing reliable sensors that create a safer, sustainable and more connected future is our ultimate goal,” said Xing Liu, product manager, TE Connectivity. “Analog infrared thermopiles measure non-contact temperature and are available with various lenses and filters, allowing for use in multiple applications, including industrial pyrometers, climate controls and medical devices.”
Additional benefits of TE’s analog infrared thermopiles for applications across the auto, aerospace, industrial, appliance and medical device sectors include:
- Measures a wide range of temperatures from -40°C to +300°C. The robust package utilizes highly accurate reference nickel RTD- or NTC-based sensors, allowing TE thermopiles to be more easily compensated and provide an accurate output.
- Multiple configurations for single pixel or multi pixel.
- Optical filter options including a standard flat window and a range of silicon lenses for a narrow field of view to filter specific wavelengths.
- Robust sensor packages including hermetically sealed housings, stainless steel packaged housings and integral circuit boards and connectors.
For more information TE’s sensors business, visit te.com/sensors.
Documentation and Additional Information
About TE
TE Connectivity is a global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions enable the distribution of power, signal and data to advance next-generation transportation, renewable energy, automated factories, data centers, medical technology and more. With more than 85,000 employees, including 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat, Instagram and X (formerly Twitter).