TE Connectivity expands IoT wireless pressure sensor offering as demand grows for advanced data acquisition for precise condition monitoring
Published
04/24/24
Media Inquiries
Winston-Salem,
N.C.
Ultra-compact, cost-effective solutions available for both short- and long-range coverage
Winston-Salem, N.C. – April 22, 2024 – The growth of IoT and its advancing ecosystem has affected condition monitoring practices and contributed to evolving predictive maintenance operations.
In today’s industrial landscape, the demand for sensors that are miniaturized, digital, low power and wireless and can operate in challenging environments has never been greater. To meet these needs, TE Connectivity (TE), a world leader in connectivity and sensors, has added two new wireless pressure sensors to its portfolio: 65xxN wireless pressure sensor, for short range coverage, and 69xxN wireless pressure sensor, for long range coverage.
“Wireless sensors revolutionize how industries monitor and respond to real-time data without the constraints of wired connections,” said Andrew Smith, product manager at TE. “TE’s newest wireless pressure sensor offerings seamlessly align with the foundational principles of Industry 4.0 and the IoT-driven smart factory model while as the same time bringing practical, efficient solutions to industrial monitoring challenges and helping to keep machinery operational.”
Designed for periodic condition monitoring, 65xxN wireless pressure sensor leverages BLE (Bluetooth® low energy) 5.3 communications, to support localized data collection and transmission. Given the widespread presence of Bluetooth® in industrial equipment, the transition to BLE sensors is both pragmatic and efficient. The 65xxN wireless pressure sensor harnesses the power of BLE technology to offer both optimal battery performance and adaptability to various pressure conditions. It is also compact in nature and designed to easily fit into tight spaces and diverse environments.
Engineered with LoRaWAN® technology, the 69xxN wireless pressure sensor offers long-range coverage over several kilometers, low power consumption enabling extended battery life, and scalability to support numerous devices within a single network. This compact sensor fits effortlessly into various environments, from tight spaces to remote infrastructures, and offers wide pressure sensing range, reducing the need for multiple sensors, and simplifying system integration. What’s more, 69xxN wireless pressure sensor’s extended battery life and customizable transmission thresholds significantly lower maintenance frequency and enhance system reliability.
With robust security features for data protection and certifications for use in hazardous areas, both the 65xxN and 69xxN series wireless pressure sensors are not only reliable, but also safe for critical applications and high-risk areas.
For more information on TE’s wireless sensor offerings, visit te.com.
Additional Links: