TE Connectivity interfaces with Texas Instruments automotive SerDes devices to transfer substantial amount of data over fewer wires in new vehicle architectures
Published
07/30/24
Media Inquiries
Media Relations:
Deanna McCoy
TE Connectivity
+1 (610) 247-2902
deanna.mccoy@te.com
BENSHEIM, Germany– July 30, 2024
TE Connectivity GEMnet connectors and cable assemblies support Texas Instruments FPD-Link™ IV devices to enable high bandwidth video links with near-zero latency
BENSHEIM, Germany– July 30, 2024 –In today’s automotive landscape, manufacturers are increasingly designing applications and architectures that call for multi-gigabits (10 Gbps+) of data to be transferred over fewer wires and longer reaches. TE Connectivity, a world leader in connectivity and sensors has equipped its GEMnet connector system to work with Texas Instruments’ FPD-Link IV SerDes semiconductors to transmit high-resolution, uncompressed video and bidirectional control over lightweight cable assemblies and connectors in the automotive environment with near-zero latency.
With the introduction of pillar-to-pillar displays, automotive infotainment panels are rapidly growing and proliferating. This increased display size and quantity necessitates car manufacturers also improve screen resolution and color depth to scale proportionally to maintain the clarity and crispness of displays that consumers have become accustomed to in their everyday lives. This requires an increased quantity of data to be transmitted and received to multiple locations across the entire vehicle passenger areas while maintaining low latencies.
TI’s FPD-Link IV high-speed automotive serializer/deserializer (SerDes) is capable of supporting high-bandwidth automotive processors for display applications including 4K, 5K, and even 8K ultra-high definition (UHD) resolution displays with advanced multi-port synchronization features, daisy chain and near-zero latency. These chips interface with TE’s GEMnet connectors, and across TE’s GEMnet cables, which are specifically designed to support Multigigabit Ethernet and SerDes applications and handle large data volumes over long runs up to 15M.
“At TE, we work with virtually every OEM and understand the complex needs of the industry as vehicle architectures continue to evolve,” said Nick Defensor, product manager at TE. “We are excited to work with Texas Instruments and use their FPD-Link IV interface chips to work alongside to our GEMnet connectors, and believe this collaboration demonstrates our commitment to offer solutions that not only support current and future vehicle requirements but also improve the driver experience.”
“TE and Texas Instruments have a long history in the automotive industry supporting global OEMs,” said Andrew Glenny, business manager for FPD-Link at Texas Instruments. “TE’s GEMnet connector working alongside our FPD-Link devices enables support for 4K and higher resolutions, with data rates over 10Gbps, which enables engineers to optimize high-speed data transfer in their automotive systems.”
TE’s GEMnet connector system offers the flexibility to support a wide range of Ethernet and SerDes applications and industry protocols including 4K displays, radar/lidar, high-resolution camera and safety-critical applications. It features 90° and 180° terminals and offers sealed and unsealed product types. Compatible with USCAR interface, TE’s GEMnet connector system can be used with a variety of different cables including shielded twisted pair, unshielded twisted pair and new high-performance cables. This provides automotive manufacturers with a high-performance connector system that can be used in a broad array of automotive applications and offers specific advantages in terms of automotive robustness, which include the robust ground contact design and integrated lead-in features and stub protection.
For more information about TE Connectivity’s high speed products and solutions, visit Automotive-Data-Connectivity-Solution | TE Connectivity.
About TE
TE Connectivity is a global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions enable the distribution of power, signal and data to advance next-generation transportation, renewable energy, automated factories, data centers, medical technology and more. With more than 85,000 employees, including 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat, Instagram and X (formerly Twitter).