Watch as engineers from TE, Avnet, and Microchip reveal a cutting-edge HVAC air flow demonstration system to demonstrate their ground-breaking collaboration. Real-time remote monitoring and cloud-based control are made possible thanks to this ground-breaking technology's smooth connections. Witness how the power to transform data into actionable insights has changed the IoT landscape. Don't miss out on this exciting demonstration video that showcases the future of connected technology.

Application
Mechanical Ventilation
Reducing a building's energy and cost while improving comfort isn’t just about efficient heating and air conditioning. The “V” in HVAC is for ventilation and mechanical ventilation, sensors are improving the efficiency of HVAC systems while keeping interior spaces comfortable and healthy.
Ventilation is required for both HVAC comfort and good air quality. Without enough ventilation, users will eventually experience comfort issues and even health problems. These could range from worker fatigue to experiencing Sick Building Syndrome in a commercial space. Experts have also recommended increasing ventilation to prevent the spread of COVID-19 by diluting virus particles. Ventilation is about adding the proper amount of fresh air from the outside to the indoor air space. Mechanical ventilation uses ducts and fans to draw in and distribute fresh air throughout a space, and sometimes to exhaust air from specific areas. Mechanical ventilation is beneficial not only for energy efficiency, but to provide more control over the amount of outdoor air added, as well as its source. To accomplish this level of control and efficiency, mechanical ventilation requires data to determine what vents to open or close, and what direction to move the air. Two newer techniques that utilize mechanical ventilation techniques include variable air volume, or VAV, and energy recovery ventilation, or ERV. Both utilize an array of sensors to ensure proper levels of airflow and the accurate temperature and humidity control. Board mount differential pressure sensors are crucial to monitoring and maintaining proper airflow for each zone and to ensure that system filters are not blocked. Duct mount and averaging temperature sensors are used to help monitor and control temperatures in each zone. Additionally, monitoring the humidity between zones and the outdoors can help maintain an ideal indoor humidity around 30 to 50%. This range is comfortable for people, while being high enough to reduce the rate of infection for viruses such as influenza and low enough to reduce the growth of microorganisms. To monitor both temperature and humidity, TE Connectivity (TE) manufactures the HTU series of sensors which provides accuracies of ±2%RH for humidity and ±0.2°C for temperature.


Join an interesting discussion on the cutting-edge field of HVAC system airflow monitoring, conducted by engineers from TE, Avnet, Microsoft Azure, and Microchip. Gain useful knowledge and participate in the discussion that examines the most recent developments in this important area. Don't miss your chance to view this engaging discussion, which is sure to produce ground-breaking approaches to monitoring and optimizing airflow.