Formulas and Calculators
Find formulas and calculators to assist you in designing your medical device.
Modelling Pushability
As pushability is related to tube longitudinal stiffness, it is calculated to be:
klong = EA/L
Where
- klong is the longitudinal spring constant,
- E is the modulus of elasticity,
- A is the cross-sectional area
- L is the length of the catheter shaft.
To maximize pushability klong must be maximised.
This can be achieved in various ways:
- By maximizing the cross-sectional area of the tubing.
- By maximizing the modulus of elasticity by using a stiffer material.
- By decreasing the overall part length.
Modelling Torqueability
Torqueability is a measure of the tubes torsional stiffness and can be modelled using:
ktorq = GJ/L
Where
- ktorq is the torsional spring constant
- G is the shear modulus
- J is the polar moment of inertia
- L is the length of the catheter shaft
Maximizing torqueability is achieved by maximizing the torsional stiffness value, ktorq, through actions that include:
- Maximizing the polar moment of inertia. For a tube, the governing equation for J is:
J= PIE/32 (d4o- d4i)
In order to maximize J, the outside diameter and the wall thickness should be maximised.
- By maximizing the shear modulus using a stiffer material.
- By decreasing the overall part length.
Modelling Flexibility
The flexibility or flexural stiffness of a tube is determined by:
kflexural = 3EI/L3
Where
- kflexural is the flexural spring constant
- E is the modulus of elasticity
- I is the moment of inertia
- L is the length of the catheter shaft.
To improve the flexibility of the tube the flexural stiffness value, kflexural, the must be minimized through actions that include:
Minimizing the moment of inertia. For a tube, the governing equation for I:
I = PIE/64 (d4o- d4i)
In order to minimize I, the wall thickness must be at a minimum:
- By minimizing the modulus of elasticity by using a soft material.
- By increasing the overall part length.
Flexibility is not however a measurement of kink resistance. Experimental Data has shown that tubes with a small ID/OD ratio perform better than those with higher ID/OD ratios. That is those with thick walls have better kink performance than those with thinner walls.
Converter Calculator
The converter calculator is an invaluable tool for any engineer – it easily converts measurements of area, force, pressure, speed, power, light etc.
Download this useful calculator from the link below.