das antenna

Choosing a Wi-Fi Antenna

Get answers relevant to Wi-Fi antenna designs.

What is a Wi-Fi Antenna?

A Wi-Fi antenna is a vital component in Wi-Fi communication systems and serves as a transmitter, receiver, or both. It enables devices to transmit and receive radio frequency (RF) waves for internet connectivity.

 

A Wi-Fi antenna operates in two possible ways: by radiating RF when provided with electric power, or by converting these radio waves back into electric power.

 

Wi-Fi antennas can vary in size and shape and are designed to accommodate effective radiation and reception within specific frequency ranges. For Wi-Fi communications, the frequencies are typically in the 2.4, 5, and 6 GHz bands.

 

Selecting a Wi-Fi antenna is determined by its intended use within the wireless network system. Wi-Fi antennas are designed to meet requirements like range, signal strength, and the types of devices being connected. 

Orange Spacer

How Do Wi-Fi Antennas Work?

Wi-Fi antennas convert radio frequency (RF) waves, which contain packets of information, into electrical signals, or electrical signals into RF.  This conversion method permits wireless devices such as routers, smartphones, laptops, and tablets to communicate wirelessly. The receiving antennas of the devices pick up RF frequencies and transform them into electrical signals that the devices process. Transmitting antennas, on theother hand, convert electrical signals back into RF for transmission.

 

Transmission Process

  • Data Encoding: A specific encoding scheme converts digital data from a device into electrical signals.
  • Signal Modulation: The electrical signals are modulated onto a carrier wave. A carrier wave is a high-frequency radio wave.
  • Antenna Radiation: The modulated carrier wave is sent into the Wi-Fi antenna. The antenna acts like a transducer by converting the electrical signal into RF frequencies that are subsequently radiated into the neighboring environment.

 

Reception Process

  • RF Reception: RF frequencies are transmitted by other devices or access points to the Wi-Fi antenna.
  • Signal Demodulation: The RF is demodulated to obtain the original electrical signals. This process includes separating the modulation carrying the data from the carrier wave.
  • Data Decoding: Applying the same encoding scheme that was used for transmission, the electrical signals are decoded back into digital data.

 

Factors That Affect Wi-Fi Antenna Performance

  • Antenna Gain: This measures an antenna’s capability to amplify a signal. Higher gain antennas give stronger signals and longer range.
  • Antenna Placement: Proper placement reduces obstruction and interference, enabling a strong signal reception and transmission.
  • Environmental Factors: Obstructions like walls and furniture can weaken Wi-Fi signal transmissions. By using strategic antenna placement and high-gain antennas, such obstacles can be mitigated. 
Orange Spacer

What are the Different Types of Wi-Fi Antennas?

The two main types of Wi-Fi antennas are omnidirectional and directional antennas.  

 

Omnidirectional antennas provide a signal in a 360-degree pattern and are intended for wide coverage in a contained area. However, these can have a shorter range than directional antennas. Omnidirectional antennas vary in size and shape dramatically. These can be extremely small chip antennas that mount directly onto a PCB and are measured in millimeters. These range all the way to large base station antennas that can be three meters or more in length and are commonly tube/baton shaped.

 

Directional antenna signals are focused in one specific direction and are suited for longer range, point-to-point, or point-to-multipoint Wi-Fi networks. These provide focused coverage over longer distances but have more limited coverage area (i.e., they do not radiate in all directions like an omnidirectional antenna).

 

Directional antennas are usually more structured in terms of shape and will often be a flat panel antenna, Yagi-type antenna, or parabolic antenna. However, this is not always the case. Directional antennas range from PCB-mounted antennas to larger examples that can be wall- or pole-mounted.  

Orange Spacer

What are Wi-Fi Antennas Used For?

Wi-Fi communication is a fundamental aspect in the day-to-day lives of almost every person who connects wirelessly today and in the future. This is true of home users accessing streaming services, web browsers, online gaming, and other activities. Wi-Fi coverage is also necessary in commercial or industrial applications where a Wireless Local Area Network (WLAN) may be in place to provide a secure and high-speed network. Examples of commercial WLAN networks are a port, large factory, or warehouse setting where high-speed data transmission is essential.

 

Wi-Fi applications are everywhere in modern technology and enable wireless connectivity and data transmission in a wide range of applications, spanning from personal devices to large-scale networks. They have revolutionized communication by their ability to transmit and receive radio signals.

Below are some examples of Wi-Fi applications.

  • Wireless Networking: Wi-Fi antennas are essential for creating network which enable devices like laptops, smartphones, and tablets to connect to the internet or each other without the use of cables.
  • Internet Access: Wi-Fi antennas provide wireless internet access that allows devices to connect to routers and access websites, cloud-based applications and online services.
  • Data Transmission: Wi-Fi antennas enable data transmission between wireless devices. This allows for file sharing, streaming services, video conferencing, and other activities.
  • Internet of Things (IoT): IoT devices like sensors, wearables, and smart home appliances connect to the internet via Wi-Fi antennas and share data, which facilitates data collection, analysis, and remote control.
  • Smart Home Automation: Wi-Fi antennas are crucial to smart home devices and allows them to connect to the internet and each other. Services include remote control, automation, and monitoring of home appliances and systems.
  • Wireless Communication Infrastructure: Wi-Fi antennas are used in wireless communication infrastructure including access points, routers, and repeaters which extend the range and coverage of Wi-Fi networks.
  • Wireless Surveillance Systems: Wireless security cameras and monitoring systems can transmit video footage and other data to remote locations for surveillance and security purposes via Wi-Fi antennas.
  • Wireless Audio and Entertainment: Products such as wireless speakers, headphones, and entertainment systems use Wi-Fi antennas to transmit audio signals without the need for cables.
Orange Spacer

What Differentiates TE Wi-Fi Antennas from Other Companies?

We offer an extensive product portfolio and expertise in antenna design and manufacturing capability built over decades. This is coupled with our commitment to innovation and quality. When it comes choosing our Wi-Fi antennas, here are factors to keep in mind:

  • Broad Portfolio: We manufacture a comprehensive range of Wi-Fi antennas for diverse applications, including indoor and outdoor use, and directional, omnidirectional, and multi-band antennas. This extensive portfolio enables customers to find the Wi-Fi antenna that can suit their needs, and custom antennas can be developed for OEM applications.
  • Advanced Technology: A leader in antenna innovation, we continuously seek to create technologies and designs to enhance antenna performance. We uses advanced techniques, including metamaterials and phased arrays, to create high-performance antennas that have exceptional gain, range, and efficiency.
  • Customization Expertise: We offer expertise in customizing antenna solutions to address client-specific requirements. Our team of experts collaborate with customers to design and manufacture antennas to match customer specifications and provide optimal performance.
  • Global Manufacturing: We operate a global network of manufacturing facilities which enables us to produce antennas near our customers. Such proximity can enable customers to receive antennas in a timely manner.
  • Quality Assurance: Our antennas address quality and reliability requirements. We follow rigorous testing procedures and use high-grade materials to help provide long-lasting performance.
  • Industry Recognition: We are known for our innovative designs and high-quality products. We have earned numerous industry awards and certifications, which have helped solidify our reputation as a trusted provider of Wi-Fi antennas.