TE Connectivity Heat Shrink Tubing
Heat Shrink Tubing, unlike many other products is designed to change shape when installed. Correctly sized tubing will conform to the substrate over which it is applied. It shrinks in diameter and in general overall length. This can make it especially tricky to select the right size for your application. This guide was put created to help with that process.
To achieve a good robust installation of heat shrink tubing it is important to get the best fit of the tubing to the substrate. To do this, the tube needs to shrink by at least 20% of its supplied size but not so far that the tube reaches its fully recovered size. It is best to have at least 10% unresolved recovery after the tube is installed.
Example: RNF-100 size 1” recovers to a maximum of 0.50”. It should be used for applications where the expected recovered size is between
Or in other words, it is intended to cover something that measures between0.55”- 0.80” outside diameters.
Will the heat shrink tubing work in the zone outside the recommended installation window? Maybe, but it will not give optimal performance.
Always select the biggest size tube that will fit the application. It will be easier to install and achieve the target wall thickness on of the installed tube. This will give a more robust solution.
                                    
                                
                                    
                                
                                    
                                
                                    
                                Just as the tubing will shrink in diameter, it will also shrink slightly in overall length during the recovery process(in general – in some case it can grow in length). Different products have different longitudinal shrinkage %’s.
Please consult with a Field Applications Engineer if this is a concern prior to
placing an order. Make sure to account for this when specifying the cut length needed or when cutting the tubing in-house. When using a long length of tubing, it will need to be cut longer than the distance it needs to cover because of the shrinkage during recovery.