Truck and excavator in operation on a construction site.

Challenges in Full-Throttle Data Connectivity

The demand for robust data connectivity in trucks and heavy equipment requires optimally engineered technologies capable of keeping equipment updated and optimized for evolving opportunities, requirements, and threats.

It’s early morning on a remote construction site in the Arizona desert. The lead engineer arrives early and immediately boots up his tablet to download the latest modifications to the project plan. It no sooner powers on when the screen goes blank, the little wheel spiraling rapidly, seconds feel like minutes, and all that time, there’s no indication of available service.

 

Sure he could have downloaded the 3D models back at his hotel so he could access the information offline on the site. But in the field, where vital updates are needed, team leaders and equipment operators need connections they can rely on, connections that work as hard as they do – and keep going until the job is finished.

 

Whether it’s a construction site, or a lonely stretch of highway, heavy-vehicle operators rely on equipment built with telematics systems that enable them to access crucial information in real-time – so they can resolve onsite material needs quickly, assess vehicle performance under extreme stress, and optimize long-haul routes effectively under ever-evolving roadway and weather conditions. When conditions are unpredictable, especially in cellular dead zones, robust, reliable connectivity matters.

The Race to 5G Connectivity

Across the U.S., the rollout of 5G connectivity faces numerous unique challenges. Not least of which is a massive geographic area with interspersed expanses of rural locations. These challenges make rollout uneven. In urban and suburban corridors, particularly along the east and west coasts, 5G delivers ultra-fast signals, but in heartland states, many still rely on 4G systems.

 

Worldwide, in 2024, telecom providers enabled 2.25B 5G connections, with North America in the lead for 5G adoption with a reported 289M 5G connections. The general expectation is that adoption will increase as 5G networks becomes more prevalent.

 

But it’s not a matter of simply enabling 5G in more places. It also involves pivoting as wireless carriers position themselves for future growth. Meaning that in the dense fields of an Iowa farm and the long stretches of highways cutting across Montana, the barriers to running outdated communications and monitoring systems in trucks and construction vehicles will drastically increase as wireless carriers shutter 3G networks.

 

As fleet owners look to the future, the top-of-mind concern is a shift toward enabling newer data-communications technologies, which means instead of merely moving from 3G to 4G, now is the time to invest in systems capable of running 5G, with an eye toward the evolution toward 6G.

Challenges in Engineering Data Connectivity

Harsh Environments

While many of the conventional physical and environmental hurdles have been resolved, such as the effect that metal components and antenna placement in trucks can have on disrupting wireless signals, fleet operators must focus on the performance impact that heavy vibration, dust, mud, and electromagnetic noise can have on complex communications technologies, particularly in off-highway equipment.

Bandwidth vs Coverage

Effective performance on the site and on the road is no longer simply about enabling a data connection, it’s increasingly about managing that connection. With trucks and heavy equipment generating terabytes of data from systems such as high-definition cameras, LiDAR scanners, and engine logs, vehicles and equipment need telematics systems capable of running advanced algorithms capable of organizing and prioritizing crucial activity and performance data and determining what can be buffered and what can be processed on the vehicle itself. By managing data through advanced communication protocols and analyzing data on the edge (in the vehicle’s own computer) and only sending summarized insights or urgent alerts over the network, fleet managers can reduce data latency, conserving available bandwidth for the most critical information.

Self Driving Tractor

Data Latency

Latency is the make-or-break factor when it comes to using communications systems effectively when the stakes are high. Even the slightest delay can escalate into a critical service disruption when heavy machinery is involved. Consider the dangers if a 20-ton robotic bulldozer were to lose its connection with its operator – even briefly – while performing an intricate task on an active work site.

 

This is why ultra-low latency communication – getting data from A to B now, not a second later – is vital for real-time operations and real-time decision making. Without it, even the most mundane operation can become much riskier if crucial hazard warning or braking commands happen too late. When thinking about vehicle-to-vehicle (V2V) connectivity used in trucks, ultra-low data latency can improve roadway operations by enabling emergency braking and lane keeping. For example, if a driver suddenly slams the brakes on his vehicle, a communications system could immediately send an alert notifying the other vehicles around the truck of the driver’s action, enabling them to respond that second sooner, which could make all the difference – but only if the available networks are fast enough and reliable enough to send that alert instantly.

Cybersecurity

With all the connectivity increasingly designed into trucks and heavy equipment, and the ever-evolving role these machines are expected to play as rolling data centers, fleet owners must prepare for a new level of theft unfamiliar to them: cyber theft. Any truck or excavator that’s connected is under threat of attack from a wide array of wrongdoers, as noted by TE’s Mark Brubaker, senior manager for business development. “After all, trucks move nearly 80% of intrastate goods and carry natural gas and fossil fuels, gasoline, foodstuffs, electronics, pharmaceuticals and more. They represent a target for bad actors who may seek to use the vehicle’s software to interrupt the flow of goods or worse. In the off-highway space, this scenario could mean construction projects are disrupted, or farming operations are impeded.”

 

In an extreme case, this could involve a nefarious act of tapping into a truck’s communications system and remotely disabling the brakes on an 18-wheeler rolling at high speed along a highway. Or more subtlety, this could involve stealing sensitive route data, making valuable cargo – from food and electronics to fuel and chemicals – vulnerable to theft at the transport destination. In either case, the outcomes could undercut trust in enabling robust data connectivity across fleet operations.

Path to Next-Generation Connectivity

In today’s hyper-connected world, bandwidth is the new horsepower. For fleet owners and operators, staying competitive means keeping equipment updated and optimized for today’s ever-evolving needs and tomorrow's opportunities, requirements, and threats. It also means working closely with the right partners who understand the evolving connectivity landscape and who can help engineer systems addressing rugged performance, edge connections, and zero-trust security. Only then can fleets achieve the reliable, predictive, and integrated communication required to operate in harsh, complex, and advanced technological environments.