![defense markets](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/story-hero-rendition/defense-collage-1024-400.jpg/jcr:content/renditions/hero-story.jpg)
Industries
Connect with Mission Critical Reliability
In combat theater situations, you can trust TE components and solutions to make the connections you rely on.
Simplifying systems and advancing capabilities. Nothing is more important on or off the battlefield than reliable military systems. They require efficient use of space without sacrificing reliability, adding unnecessary weight or compromising mission effectiveness. TE Connectivity (TE)'s expertise in interconnection products and systems helps ensure complete system compatibility for challenging applications in defense environments. Complexity of weapons systems, power distribution, networking and soldier systems is growing rapidly. TE helps to simplify interconnections, increase performance, and enhance reliability to achieve greater accuracy, faster response and better communications.
Ground Defense
Rugged Components
Interconnects to Keep and Maintain Mission Readiness
Ground defense not only presents challenging environments, it also requires heightened system compatibility. Our components offer superior electrical interconnection performance under these extremely rugged conditions.
![Ground Defense Weapons](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/soldiersystems/ground_defense_weapons_300x250.jpg)
![Ground Defense Vetronics](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/soldiersystems/ground_defense_vetronics_300x250.jpg)
Power Distribution
Tap Powerful Solutions
TE Connectivity (TE) offers relays and contacts with make/break current ratings up to 2000 A, current ratings up to 1000 A at 28 VDC and 500 A at 900 VDC, and hermetic sealing for reliability. Our relays offer one of the industry’s leading combination of high current switching in compact, lightweight packages.
Weapons Systems
Simplifying Systems, Advancing Capabilities
As the complexity of weapons systems increases, we help simplify interconnections, increase performance, and enhance reliability to achieve greater accuracy, faster response, and better communications.
Military Aerospace
Aerospace Power and Control
Smarter Connectivity for Intelligent Flight Control
We understand the complex system protocols, key electrical parameter requirements, and overall mechanical performance requirements of the military aerospace market.
As you look toward a holistic approach to system integration, count on TE for solutions and expertise in every system from avionics and flight control, to power and weapons systems, to electronic warfare and unmanned aerial vehicles.
![Military Aerospace](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/soldiersystems/mil_aero_620x250.jpg)
Fixed and Rotary Wing
Setting new direction in flight control
Modern flight controls combine mechanical, hydraulic, and increasingly fly-by-wire systems to manage flight control surfaces, landing gear, and other mechanisms. As the sophistication of these controls increases, so do the requirements for faster processing speeds and smaller, lighter, and more reliable solenoids, sensors, and actuators.
Success in today’s rugged avionics environment is more than a thorough understanding of your own products. Success demands an equally sophisticated understanding of the application and how well your product interacts as part of an overall integrated system. At TE, we understand complex system protocols, key electrical parameter requirements, and overall mechanical performance requirements of the military aerospace market.
Military Marine
The sea is a harsh environment, ever challenging the electrical and electronic systems that control naval vessels. With our deep understanding of the unique needs of marine environments, TE Connectivity (TE) has a proud history of providing solutions to make ships more reliable, more sophisticated, and mission ready. Our solutions save weight, require less space, and help you achieve new levels of performance. Whether it’s processing-intensive target acquisition or reliable delivery of power, you’ll find more choice of seaworthy products to support the mission undersea, in littoral waters, or across the expanses of oceans.
![Military Vessels](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/soldiersystems/mil_marine_300x250.jpg)
![Military Ships](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/soldiersystems/mil_marine3_300x250.jpg)
Military Marine Solutions
Tame a Harsh Environment
TE Connectivity's (TE) product range supports defense-related harsh environment applications and has a long history of designing and building military connectors and system solutions. Products designed to perform in both littoral, as well as very deep water applications, across a range of government platforms including submarines, surface ships, helicopters, ground vehicles, AUVs, ROVs, and UUVs.
Marine Weapons & Payload
Launch the mission with critical reliability
Whether it’s processing-intensive target acquisition or reliable delivery of power, you’ll find more choice of seaworthy products to support the mission undersea, in littoral waters or across the expanses of oceans.
Propulsion & Power Distribution
Rely on High Performance Power Control
Our power distribution solutions may help combat the potential hazards of naval applications, resisting salt, moisture, harsh oils, fuels, and other solvents and maintaining efficient power distribution under tough conditions of vibration and shock.
Hull Electrical
Built in Reliability from Bow to Stern
TE is boosting performance with powerful infrastructure solutions. You will find cables with reduced size and weight, sealed relays and contactors and a wide assortment of products to help manage and identify cables and subsystems
Missile Defense
Compact and Intelligent Design
Survivable Solutions in Harsh Environments
TE is helping designers create missile defense systems that are smarter, smaller, lighter, and more reliable. While a missile needs only to work once, every missile must be ready to perform.
![Missile Defense](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/soldiersystems/missile_defense_620x250.jpg)
Seeker Guidance
Bandwidth for Precision Targeting
As the sophistication of sensors grows and systems use multiple sensors, the data they provide becomes more complex. Connectivity to handle the data is moving from Gigabit Ethernet to 10G in networking, while signal processing systems need to pack more bandwidth into smaller packages.
Warheads
Mission Critical Reliability
Our connectors are designed for quick and reliable release of the store from the aircraft. Reliability is maximized with TE precision relays and timers to help confirm the payload is delivered on target.
Control Systems
Making it Work Together Flawlessly
Flight controls must monitor airframe dynamics and adjust flight parameters. Control systems deal with every section of the missile. They must be well protected against EMI, not only generated within the system but from external countermeasure sources.
TE is helping designers create missile defense systems that are smarter, smaller, lighter, and more reliable. While a missile needs only to work once, every missile must be ready to perform flawlessly at a moment’s notice. All subsystems must be reliable and easily maintainable to keep the missile mission ready.
Space
Lightweight Design for Extreme Conditions
Launch Reliability for The Final Frontier
Space applications mean extreme conditions and demand the best in lightweight composition, innovative design and reliability.
![Space Launch](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/soldiersystems/space_300x250.jpg)
![Satellite Systems](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/soldiersystems/space2_300x250.jpg)
Space Launch Vehicle
Connectivity from Launch to Target
Umbilical connectors, wire, cable, relays, contactors, sensors, Mil-Std-1553 databus and a host of avionics interconnect make TE a world leader in launch vehicle connectivity.
Space Craft Chassis
Making it work in Zero G
TE provides high tech, high reliability solutions for spacecraft chassis and satellite buses, including data and power interconnect, sensors, power distribution devices like relays and contactors, space compatible wire, cable and integrated systems, such as Mil-Std-1553 databus.
Space C4ISR
TE offers a broad portfolio of Space qualified and Space compatible connectivity solutions, including inside-the-box and box-to-box solutions that are light weight, high bandwidth and space friendly.
Soldier Systems/Wearables
Military Communication Systems
Enabling the Connected Soldier
Electrical interconnects made smaller, lighter, and more modular, mission specific configurations.
![Connected Soldier Systems](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/soldiersystems/soldier_systems_620x250.jpg)
-
O.C.H. Micro Circular Connectors
US Army approved circular connectors
Soldier and Weapons System
Enabling the Connected Soldier
Operating in adverse conditions requires soldier systems that are not only rugged, but also easy to use. TE offers a range of interconnect solutions that are ergonomic, yet reliably rugged, and that save space and weight when every ounce counts.
Equipping soldiers for modern missions means giving them the technological edge to succeed. You need to integrate personal networks, sensors, C4 communications, and the power to manage the systems. And you need to connect all the systems in a reliable and easy to use manner.
Unmanned Vehicles (UAV)
Intelligent Remote Communication Systems
Fly Higher, Stay Longer
Unmanned aerial systes, ranging from 60-foot wing spans on high altitude platforms to the size of a small hummingbird, require innovative solutions to meet the mission requirements of long flight times, advanced intelligence-gathering capabilities, and weapons delivery.
![UAV Systems](/content/dam/te-com/images/aerospace-defense-and-marine/defense/global/soldiersystems/uav_620x250.jpg)
Unmanned vehicles have become an important mainstay in modern battle spaces, and next-generation systems will continue to be required to do more with less size, weight, and power consumption (SWaP). Reducing SWaP is vital to longer mission deployments, greater fuel efficiency, and the ability to add additional surveillance and combat capabilities.