Application
Enabling fronthaul to backhaul and beyond
Our base station and optical transport connectivity solutions address the demands of the always-on edge of expanding wireless infrastructure.
Along with increased capacity demands driven by the explosion of cloud and connected device growth, engineers need interconnects that enhance the design, implementation, and maintenance of networks from the access point to the core. Our innovations in connectivity technologies push the boundaries of speed and bandwidth within today’s architectures and address challenging data rate, signal, and power requirements of 5G mobile networks. TE’s solutions also include antenna expertise, as well as high-speed board-to-board and cabled interconnects offering increased bandwidth for backplanes and midplanes.
- I/O performance is the top priority for metro & core networks. Maximize your density & speed with TE’s pluggable I/O connector and cages which support standard interfaces for data rates up to 100G.Read More
- From bus bar to cable, hot pluggability and blind mating—we offer robust power solutions for almost any design configuration.Read More
- Our latest high-speed, high-density interconnects support a range of functions for the latest BBU and OT designs.Read More
- A range of leading IC sockets and robust memory sockets allows designers to find the best product for their system requirements.Read More
- Supporting the latest standards and engineered for 10 and 25 Gbps and beyond. Custom solutions also available.Read More
- State-of-the-art measurement solutions for improved monitoring and increased control.Read More
- A resistor is a passive component that reduces voltage or limits the current flowing through a circuit. This component can also absorb energy and dissipate this energy in the form of heat. Its resistance to the flow of electrons is determined by the conductive materials with which it is built. The materials used in the composition of a resistor perform a critical role in enabling performance reliability and stability, particularly for high-voltage, high-power, high stability/accuracy, or high-current applications.Read More
- Our high-performance switches are cost-effective, reliable, and designed to withstand extreme shock, vibration, temperature, and altitude. These products are engineered for use in robotics, control panels, motion control systems, lighting, building systems, HVAC, appliances, and an array of safety-critical applications. We also offer an extensive range of accessories, including knobs, caps, boot seals, and respective hardware.Read More
- I/O performance is the top priority for metro & core networks. Maximize your density & speed with TE’s pluggable I/O connector and cages which support standard interfaces for data rates up to 100G.Read More
- From bus bar to cable, hot pluggability and blind mating—we offer robust power solutions for almost any design configuration.Read More
- Our latest high-speed, high-density interconnects support a range of functions for the latest BBU and OT designs.Read More
- A range of leading IC sockets and robust memory sockets allows designers to find the best product for their system requirements.Read More
- Supporting the latest standards and engineered for 10 and 25 Gbps and beyond. Custom solutions also available.Read More
- State-of-the-art measurement solutions for improved monitoring and increased control.Read More
- A resistor is a passive component that reduces voltage or limits the current flowing through a circuit. This component can also absorb energy and dissipate this energy in the form of heat. Its resistance to the flow of electrons is determined by the conductive materials with which it is built. The materials used in the composition of a resistor perform a critical role in enabling performance reliability and stability, particularly for high-voltage, high-power, high stability/accuracy, or high-current applications.Read More
- Our high-performance switches are cost-effective, reliable, and designed to withstand extreme shock, vibration, temperature, and altitude. These products are engineered for use in robotics, control panels, motion control systems, lighting, building systems, HVAC, appliances, and an array of safety-critical applications. We also offer an extensive range of accessories, including knobs, caps, boot seals, and respective hardware.Read More
Input/Output (I/O)
I/O performance is the top priority for metro & core networks. Maximize your density & speed with TE’s pluggable I/O connector and cages which support standard interfaces for data rates up to 100G.
Input/Output (I/O)
SFP/SFP+ Connectors
SFP+ interconnect system supports data rates of 10 Gbps signal speeds and is backward compatible with SFP. Many cage configurations offered provide excellent shielding options.

Input/Output (I/O)
QSFP/zQSFP+ Connectors
Our quad small form factor pluggable (QSFP) portfolio of interconnects offers a large range of simple and customizable design options.

Input/Output (I/O)
RJ point five Connectors
This next-gen Ethernet link offers higher density solutions for a competitive total cost of ownership per port.

Input/Output (I/O)
RJ45 Connectors
Our jacks and plugs offer reliable and space saving solutions for flexible and time-saving installation, even in harsh environments.

Power Connectors
From bus bar to cable, hot pluggability and blind mating—we offer robust power solutions for almost any design configuration.
Power Connectors
Open Compute Project (OCP) Power Connectors
We offer the only solution fully compatible with the Open Rack V1 and V2 specifications.

Power Connectors
ELCON Mini Connectors
These interconnects provide confidence in system performance with their low resistance, highly reliable interface.

Power Connectors
RAPID LOCK Connectors
No install tools required for this fast, reliable replacement for power lugs.

INTERNAL INTERCONNECTS
Our latest high-speed, high-density interconnects support a range of functions for the latest BBU and OT designs.
INTERNAL INTERCONNECTS
Fine Pitch Board-to-Board
0.4 mm pitch connectors plus new shielded board-to-FPC solutions.

INTERNAL INTERCONNECTS
Free Height Connectors
These versatile connectors are useful for downsizing applications that require parallel stacked circuit boards.

INTERNAL INTERCONNECTS
M.2 NGFF Connectors
Save more than 20% of PCB real estate compared to the PCI Express Mini Card.

INTERNAL INTERCONNECTS
Z-PACK Slim UHD
High-Speed Connectors Designed to be among the densest connectors with the smallest possible footprint to free up valuable PCB space.
INTERNAL INTERCONNECTS
Board Level Shielding (BLS)
EMI shields that minimize crosstalk in tightly designed systems. Off-the-shelf and custom solutions available.

INTERNAL INTERCONNECTS
RF Connectors
A wide array of RF and standard coax connectors for any size base station.

INTERNAL INTERCONNECTS
Flexible Printed Circuit (FPC)
Space-saving, angled insertion connectors that can be placed in a wide range of PCB locations.

IC and MEMORY SOCKETS
A range of leading IC sockets and robust memory sockets allows designers to find the best product for their system requirements.
IC and MEMORY SOCKETS
Land grid array (LGA) Sockets
Socket technology for some of the most sought after microprocessor packages in the industry.

IC and MEMORY SOCKETS
DDR4 DIMM Connectors
Space savings, reduced height, improved power consumption, and higher data rates than the DDR3.

Cable Assemblies
Supporting the latest standards and engineered for 10 and 25 Gbps and beyond. Custom solutions also available.
Cable Assemblies
FullAXS Mini Connectors
Next generation WiMAX and x-TTA connectivity designs require slim but rugged and easy-to-install cable assemblies for outdoor use.

Cable Assemblies
Pluggable I/O Cable Assemblies
From RJ and SFP to microQSFP, TE’s high speed pluggable I/O copper cable assemblies are engineered for 25 Gbps and beyond.

Sensors
State-of-the-art measurement solutions for improved monitoring and increased control.
Sensors
Humidity Sensors
Maintain optimal and efficient environments for people and equipment.

Sensors
Temperature Sensors
Accurate temperature monitoring for greater energy efficiency.

Resistors
A resistor is a passive component that reduces voltage or limits the current flowing through a circuit. This component can also absorb energy and dissipate this energy in the form of heat. Its resistance to the flow of electrons is determined by the conductive materials with which it is built. The materials used in the composition of a resistor perform a critical role in enabling performance reliability and stability, particularly for high-voltage, high-power, high stability/accuracy, or high-current applications.
Resistors
Through-Hole Resistors
A through-hole resistor is a fixed resistor that has long, pliable leads that can be stuck into a breadboard or hand- or wave-soldered into a printed circuit board. A through-hole resistor is used to reduce the flow of electrical current within a circuit. It’s commonly composed of carbon film, metal film, metal oxide film, thick film, or wirewound.

Resistors
Surface Mount Resistors
A surface mount resistor is a tiny rectangular ceramic body with silver conductive edges on either end. They provide the same functionality as the more traditional axially leaded resistors but has a lower power dissipation capacity and oftentimes a lower stray inductance and capacity.

Resistors
Trimmers
A trimmer resistor is a type of variable resistor or adjustable potentiometer that can adjust, tune, and calibrate circuits. It is meant to never be seen or adjusted by the device’s user.

Switches
Our high-performance switches are cost-effective, reliable, and designed to withstand extreme shock, vibration, temperature, and altitude. These products are engineered for use in robotics, control panels, motion control systems, lighting, building systems, HVAC, appliances, and an array of safety-critical applications. We also offer an extensive range of accessories, including knobs, caps, boot seals, and respective hardware.
Switches
Tactile Switches
Tactile switches provide tactile feedback to the user when the switch or button makes contact with the control panel underneath, which is usually a printed circuit board.

Switches
DIP & SIP Switches
A DIP switch is a manual electronic package that is composed of a series of tiny switches. It has a rectangular casing and two parallel rows of connecting terminals. A SIP switch is a computer chip package that has a single row of connection pins.


Application
Enabling fronthaul to backhaul and beyond
Our base station and optical transport connectivity solutions address the demands of the always-on edge of expanding wireless infrastructure.
Along with increased capacity demands driven by the explosion of cloud and connected device growth, engineers need interconnects that enhance the design, implementation, and maintenance of networks from the access point to the core. Our innovations in connectivity technologies push the boundaries of speed and bandwidth within today’s architectures and address challenging data rate, signal, and power requirements of 5G mobile networks. TE’s solutions also include antenna expertise, as well as high-speed board-to-board and cabled interconnects offering increased bandwidth for backplanes and midplanes.
- I/O performance is the top priority for metro & core networks. Maximize your density & speed with TE’s pluggable I/O connector and cages which support standard interfaces for data rates up to 100G.Read More
- From bus bar to cable, hot pluggability and blind mating—we offer robust power solutions for almost any design configuration.Read More
- Our latest high-speed, high-density interconnects support a range of functions for the latest BBU and OT designs.Read More
- A range of leading IC sockets and robust memory sockets allows designers to find the best product for their system requirements.Read More
- Supporting the latest standards and engineered for 10 and 25 Gbps and beyond. Custom solutions also available.Read More
- State-of-the-art measurement solutions for improved monitoring and increased control.Read More
- A resistor is a passive component that reduces voltage or limits the current flowing through a circuit. This component can also absorb energy and dissipate this energy in the form of heat. Its resistance to the flow of electrons is determined by the conductive materials with which it is built. The materials used in the composition of a resistor perform a critical role in enabling performance reliability and stability, particularly for high-voltage, high-power, high stability/accuracy, or high-current applications.Read More
- Our high-performance switches are cost-effective, reliable, and designed to withstand extreme shock, vibration, temperature, and altitude. These products are engineered for use in robotics, control panels, motion control systems, lighting, building systems, HVAC, appliances, and an array of safety-critical applications. We also offer an extensive range of accessories, including knobs, caps, boot seals, and respective hardware.Read More
- I/O performance is the top priority for metro & core networks. Maximize your density & speed with TE’s pluggable I/O connector and cages which support standard interfaces for data rates up to 100G.Read More
- From bus bar to cable, hot pluggability and blind mating—we offer robust power solutions for almost any design configuration.Read More
- Our latest high-speed, high-density interconnects support a range of functions for the latest BBU and OT designs.Read More
- A range of leading IC sockets and robust memory sockets allows designers to find the best product for their system requirements.Read More
- Supporting the latest standards and engineered for 10 and 25 Gbps and beyond. Custom solutions also available.Read More
- State-of-the-art measurement solutions for improved monitoring and increased control.Read More
- A resistor is a passive component that reduces voltage or limits the current flowing through a circuit. This component can also absorb energy and dissipate this energy in the form of heat. Its resistance to the flow of electrons is determined by the conductive materials with which it is built. The materials used in the composition of a resistor perform a critical role in enabling performance reliability and stability, particularly for high-voltage, high-power, high stability/accuracy, or high-current applications.Read More
- Our high-performance switches are cost-effective, reliable, and designed to withstand extreme shock, vibration, temperature, and altitude. These products are engineered for use in robotics, control panels, motion control systems, lighting, building systems, HVAC, appliances, and an array of safety-critical applications. We also offer an extensive range of accessories, including knobs, caps, boot seals, and respective hardware.Read More
Input/Output (I/O)
I/O performance is the top priority for metro & core networks. Maximize your density & speed with TE’s pluggable I/O connector and cages which support standard interfaces for data rates up to 100G.
Input/Output (I/O)
SFP/SFP+ Connectors
SFP+ interconnect system supports data rates of 10 Gbps signal speeds and is backward compatible with SFP. Many cage configurations offered provide excellent shielding options.

Input/Output (I/O)
QSFP/zQSFP+ Connectors
Our quad small form factor pluggable (QSFP) portfolio of interconnects offers a large range of simple and customizable design options.

Input/Output (I/O)
RJ point five Connectors
This next-gen Ethernet link offers higher density solutions for a competitive total cost of ownership per port.

Input/Output (I/O)
RJ45 Connectors
Our jacks and plugs offer reliable and space saving solutions for flexible and time-saving installation, even in harsh environments.

Power Connectors
From bus bar to cable, hot pluggability and blind mating—we offer robust power solutions for almost any design configuration.
Power Connectors
Open Compute Project (OCP) Power Connectors
We offer the only solution fully compatible with the Open Rack V1 and V2 specifications.

Power Connectors
ELCON Mini Connectors
These interconnects provide confidence in system performance with their low resistance, highly reliable interface.

Power Connectors
RAPID LOCK Connectors
No install tools required for this fast, reliable replacement for power lugs.

INTERNAL INTERCONNECTS
Our latest high-speed, high-density interconnects support a range of functions for the latest BBU and OT designs.
INTERNAL INTERCONNECTS
Fine Pitch Board-to-Board
0.4 mm pitch connectors plus new shielded board-to-FPC solutions.

INTERNAL INTERCONNECTS
Free Height Connectors
These versatile connectors are useful for downsizing applications that require parallel stacked circuit boards.

INTERNAL INTERCONNECTS
M.2 NGFF Connectors
Save more than 20% of PCB real estate compared to the PCI Express Mini Card.

INTERNAL INTERCONNECTS
Z-PACK Slim UHD
High-Speed Connectors Designed to be among the densest connectors with the smallest possible footprint to free up valuable PCB space.
INTERNAL INTERCONNECTS
Board Level Shielding (BLS)
EMI shields that minimize crosstalk in tightly designed systems. Off-the-shelf and custom solutions available.

INTERNAL INTERCONNECTS
RF Connectors
A wide array of RF and standard coax connectors for any size base station.

INTERNAL INTERCONNECTS
Flexible Printed Circuit (FPC)
Space-saving, angled insertion connectors that can be placed in a wide range of PCB locations.

IC and MEMORY SOCKETS
A range of leading IC sockets and robust memory sockets allows designers to find the best product for their system requirements.
IC and MEMORY SOCKETS
Land grid array (LGA) Sockets
Socket technology for some of the most sought after microprocessor packages in the industry.

IC and MEMORY SOCKETS
DDR4 DIMM Connectors
Space savings, reduced height, improved power consumption, and higher data rates than the DDR3.

Cable Assemblies
Supporting the latest standards and engineered for 10 and 25 Gbps and beyond. Custom solutions also available.
Cable Assemblies
FullAXS Mini Connectors
Next generation WiMAX and x-TTA connectivity designs require slim but rugged and easy-to-install cable assemblies for outdoor use.

Cable Assemblies
Pluggable I/O Cable Assemblies
From RJ and SFP to microQSFP, TE’s high speed pluggable I/O copper cable assemblies are engineered for 25 Gbps and beyond.

Sensors
State-of-the-art measurement solutions for improved monitoring and increased control.
Sensors
Humidity Sensors
Maintain optimal and efficient environments for people and equipment.

Sensors
Temperature Sensors
Accurate temperature monitoring for greater energy efficiency.

Resistors
A resistor is a passive component that reduces voltage or limits the current flowing through a circuit. This component can also absorb energy and dissipate this energy in the form of heat. Its resistance to the flow of electrons is determined by the conductive materials with which it is built. The materials used in the composition of a resistor perform a critical role in enabling performance reliability and stability, particularly for high-voltage, high-power, high stability/accuracy, or high-current applications.
Resistors
Through-Hole Resistors
A through-hole resistor is a fixed resistor that has long, pliable leads that can be stuck into a breadboard or hand- or wave-soldered into a printed circuit board. A through-hole resistor is used to reduce the flow of electrical current within a circuit. It’s commonly composed of carbon film, metal film, metal oxide film, thick film, or wirewound.

Resistors
Surface Mount Resistors
A surface mount resistor is a tiny rectangular ceramic body with silver conductive edges on either end. They provide the same functionality as the more traditional axially leaded resistors but has a lower power dissipation capacity and oftentimes a lower stray inductance and capacity.

Resistors
Trimmers
A trimmer resistor is a type of variable resistor or adjustable potentiometer that can adjust, tune, and calibrate circuits. It is meant to never be seen or adjusted by the device’s user.

Switches
Our high-performance switches are cost-effective, reliable, and designed to withstand extreme shock, vibration, temperature, and altitude. These products are engineered for use in robotics, control panels, motion control systems, lighting, building systems, HVAC, appliances, and an array of safety-critical applications. We also offer an extensive range of accessories, including knobs, caps, boot seals, and respective hardware.
Switches
Tactile Switches
Tactile switches provide tactile feedback to the user when the switch or button makes contact with the control panel underneath, which is usually a printed circuit board.

Switches
DIP & SIP Switches
A DIP switch is a manual electronic package that is composed of a series of tiny switches. It has a rectangular casing and two parallel rows of connecting terminals. A SIP switch is a computer chip package that has a single row of connection pins.